JAJSGD8B October 2018 – Sept 2019 TMUX1574
PRODUCTION DATA.
The parasitic capacitance of the device is captured at the source (Sx), drain (Dx), and select (SELx) pins. The capacitance is measured in both the on and off state and is denoted by the symbol CON and COFF. Figure 38 shows the setup used to measure capacitance.
Figure 38. Capacitance Measurement Setup