DLPU082C August 2021 – March 2024 DLPC7540
Set Initialize On The Fly Load Splash Image | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0-19 |
Header of the pattern Image (same format as the splash header) |
Bytes 20-21 |
Width of the splash image, in pixels, to which given pattern is to be replicated |
Bytes 22-23 |
Height of the splash image, in pixels, to which given pattern is to be replicated |
This Command Initializes the on the fly splash load operation. It is used to give the information about the image (dimensions, pixel format, compression used and so on) and sets the data path for the splash load operation. It also resets prior operations. It should be called once before loading an image on the fly. |
Set Load Splash Image On The Fly | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0 - * |
Image Data |
This Command receives the image data and writes it into the VPS DRAM Buffer. It performs decompression if required. Due to the limitation of USB, the entire image data may not be sent in one go. Hence, this command has to be called multiple times to load the entire image. It also stores any bytes that are unprocessed by the API (if the API does not have all the bytes required to perform an operation). These unprocessed bytes are sent over to callback function the next time data is received. The API displays the loaded splash once the entire image is loaded into the memory. The remaining pixels to load the image is also returned by the callback function. |
Set XPR Calibration Pattern Display | |
---|---|
Write Parameters | |
This command loads a pre-defined XPR Calibration pattern as a splash image and displays it on the screen. A 64x64 pattern is repeated over a 3840x2160 display area. |
Set XPR 4Way Orientation | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
Orientation number. Range 0 - 23. |
This command sets the orientation number of the actuator position (which gets stored in EEPROM) There are 24 possible options 0 - 23; use this command while performing XPR calibration using TI provided XPR calibration splash image. Note : Use Display Image Size command to make sure the display area is 3840x2160 If the reported display resolution is less than or equal to 1080p this command will not have any influence on the displayed image. |
Get XPR 4Way Orientation | |
---|---|
Data returned is in the same format as the Write Parameters. | |
This command retrieves the last set orientation number or the subframe order |
Set XPR Actuator Waveform Control Parameter | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
XPR Command 0 = Fixed Output Enable 1 = DAC Gain 2 = Subframe delay 3 = Actuator Type (READ ONLY) 4 = Output Enable/Disable 5 = Clock Width 6 = DAC Offset 7 = Number of Segments 8 = Segment Length 9 = Invert PWM A 10 = Invert PWM B 11 = Subframe Filter Value 12 = Subframe Watch Dog 13 = Fixed Output Value |
Byte 1 |
Channel number (0 or 1) of Actuator waveform control for which the command parameter has to be applied |
Bytes 2-5 |
Data that needs to be passed to the command |
This command configures/sets up the Actuator Waveform Control(AWC) block. Here, AWCx can be AWC 0 or 1. Bytes 2-5 contains the XPR command data as mentioned in Byte 0. Byte 1 contains AWC channel number, possible values are 0 or 1. Fixed Output Enable : Configures Actuator in fixed output mode. Byte 2 : 0x00 - Disable 0x01 - Enable Bytes 3-5 : Reserved must be set to 0x000000 Gain : Set Waveform Generator DAC/PWM Gain. Byte 2 : Range 0 - 255 format u1.7 (0 to 1.9921875) Bytes 3-5 : Reserved must be set to 0x000000 Subframe delay : Subframe delay Bytes 2-5; Range 0 - 262143 and lsb = 133.333ns Actuator Type (READ ONLY) : Actuator type Byte 2 : 0x00 - NONE 0x01 - Optotune (XPR-25 Model) 0x80 - TI Actuator Interface (EEPROM) 0x81 - TI Actuator Interface (MCU) Bytes 3-5 : Reserved must be set to 0x000000 Output Enable/Disable : Actuator output enable/disable Byte 2 : 0x00 - Disable 0x01 - Enable Bytes 3-5 : Reserved must be set to 0x000000 Note : Both AWC0 and AWC1 disabled/enabled together Clock Width : Defines the high and low width for the output clock (the clock period will be 2*(ClkWidth+1)) 0 = 1 (Clock period is two clocks); lsb = 8.33ns Bytes 2-5 : ClkWidth Example : ClkWidth = 0; will generate clock of 2*(0+1)*8.33 = 16.66ns Offset : DAC/PWM Output Offset Byte 2 : Range -128 - +127 format S7 (-128 to +127) Bytes 3-5 : Reserved must be set to 0x000000 Number of Segments : Defines number of segments Byte 2 : Range 2 - 255 Bytes 3-5 : Reserved must be set to 0x000000 Segments Length : Defines size of the segments Bytes 2-3 : Range 19 - 4095 Bytes 4-5 : Reserved must be set to 0x0000 Invert PWM A : Applicable when AWC is configured to PWM type instead of DAC Byte 2 : 0x00 - No inversion 0x01 - Inverted Bytes 3-5 : Reserved must be set to 0x000000 Invert PWM B : Applicable when AWC is configured to PWM type instead of DAC Byte 2 : 0x00 - No inversion 0x01 - Inverted Bytes 3-5 : Reserved must be set to 0x000000 Subframe Filter Value : Sets Subframe Filter Value - defines the minimum time between Subframe edges. Edges closer than the set value will be filtered out Byte 2 : 0 = Filter disabled, 0 = Filter time will be Val x 60us, Range : 0 - 255 Bytes 3-5 : Reserved must be set to 0x000000 Subframe Watch Dog : Defines the maximum time between Subframe edges; if timer expires, then the WG will automatically output the Fixed Output value, and the normal output will resume on the next subframe edge. Bytes 2-3 : 0 = Subframe watchdog disabled, 0 = Watchdog time will be Time x 60us, Range : Range : 0 - 1023 Bytes 4-5 : Reserved must be set to 0x0000 Fixed Output Value : Defines the value to be output on DAC/PWM when fixed output mode is selected. Byte 2 : Value to be output on DAC/PWM, Range -128 to 127 Bytes 3-5 : Reserved must be set to 0x000000 Note : To use Subframe Filter Value and Subframe Watch Dog care must be taken to set a value which approximately 10% more than 2x of the operating frequency. For example - 4K @ 60Hz, the value can be set as (1/(60*2))*1.10*10^6 = 9166us. |
Get XPR Actuator Waveform Control Parameter | |
---|---|
Read Parameters | |
Byte | Description |
Byte 0 |
XPR Command 0 = Fixed Output Enable 1 = DAC Gain 2 = Subframe delay 3 = Actuator Type (READ ONLY) 4 = Output Enable/Disable 5 = Clock Width 6 = DAC Offset 7 = Number of Segments 8 = Segment Length 9 = Invert PWM A 10 = Invert PWM B 11 = Subframe Filter Value 12 = Subframe Watch Dog 13 = Fixed Output Value |
Byte 1 |
Channel number of Actuator waveform control block for which the command parameter to be readback |
Return Parameters | |
Byte | Description |
Bytes 0-3 |
Parameter value obtained for the command passed |
This command gets the parameter set to the AWC waveform generator. Note : This command is supposed to be used only during the normal operating mode and not during the standby state. |
Set DB Border Configuration | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0-1 |
number of lines top of border. Range 0 - 4095 |
Bytes 2-3 |
number of lines bottom of border. Range 0 - 4095 |
Bytes 4-5 |
number of pixels of left border. Range 0 - 4095 |
Bytes 6-7 |
number of pixels of right border. Range 0 - 4095 |
This command configures area of the DynamicBlack border region for the border exclusion function. The border exclusion function allows the user to reduce the letterbox (black border) effect on a primarily bright image where letterbox area reduces the overall scene brightness for the algorithm. It also helps the algorithm better handle images with bright subtitles where the subtitles increase the overall scene brightness. This command will also be used in a multi-controller configuration to exclude any image overlap required for other image processing algorithms. |
Get DB Border Configuration | |
---|---|
Data returned is in the same format as the Write Parameters. | |
This Command returns the border region area for the DynamicBlack border exclusion function. |
Set DB Border Weight | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
Weight value of border pixels 0 = 0% weighted; 1 = 25% weighted; 2 = 50% weighted; 3 = 75% weighted 0 = Weighted 0% 1 = Weighted 25% 2 = Weighted 50% 3 = Weighted 75% |
Get DB Border Weight | |
---|---|
Data returned is in the same format as the Write Parameters. | |
Sets weight value of the DynamicBlack border region for the border exclusion function |
Set DB Clip Pixels | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0-1 |
Number of pixels that can be clipped. Range = 0 to 65535. |
This command returns currently configured number of steps to allow the DynamicBlack aperture to move. |
Get DB Clip Pixels | |
---|---|
Data returned is in the same format as the Write Parameters. | |
This command returns the currently selected number of pixels that can be clipped. |
Set DB Gain | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0-1 |
Gain value. Typical value range is 1.0 to 8.0. Format = u4.12 |
This command controls the DynamicBlack gain value. Typical value range is 1.0 to 8.0. Manual Mode needs to be enabled to set the gain as it will override the gain value that is calculated every frame. |
Get DB Gain | |
---|---|
Data returned is in the same format as the Write Parameters. | |
This command gets the DynamicBlack gain value. Typical value range is 1.0 to 8.0 |
Get DB Histogram | |
---|---|
Return Parameters | |
Byte | Description |
Bytes 0-135 |
Start address of the DB histogram array. Array size is 34. The LSB of each bin represents 32 pixels. Each bin saturates at 0x0003FFFF. |
This command returns the start address of the DynamicBlack(DB) histogram data. The histogram contains scene brightness data from the previous frame. The DB histogram contains 34 bins measuring non-overlapping intensity ranges in the displayed image. The value of each bin equals the number of pixels within the bin's intensity range. Each pixel's intensity is calculated as the maximum of its red, green, and blue values. In other words, pixel intensity = MAX( R, G, B ). Each pixel has a format of unsigned 8.8, making 16 bit values. Bins 32 and 33 are special bins that represent pixels that have values of exactly zero and only fractional values respectively. This function can be used independently of aperture control for image improvement in dark scenes. |
Get Current Led Color Point | |
---|---|
Return Parameters | |
Byte | Description |
Bytes 0-1 |
Chromatic x coordinate in (Transmitted in u1.15 format) Format = u1.15 |
Bytes 2-3 |
Chromatic y coordinate in (Transmitted in u1.15 format) Format = u1.15 |
Bytes 4-7 |
Luminance Y coordinate |
Gets x,y coordinates of system's current white point. WPC should be initialized and calibration data should be set before calling this command. |
Set WPC Optimal Duty Cycle | |
---|---|
Write Parameters | |
Searches available duty cycles and sets the optimal one for correct LED white point. Sensor calibration Data should be set before using this command. |
Get WPC Optimal Duty Cycle | |
---|---|
Return Parameters | |
Byte | Description |
Bytes 0-1 |
Red Ideal Duty Cycle (Transmitted in u8.8 format) Format = u8.8 |
Bytes 2-3 |
Green Ideal Duty Cycle (Transmitted in u8.8 format) Format = u8.8 |
Bytes 4-5 |
Blue Ideal Duty Cycle in (Transmitted in u8.8 format) Format = u8.8 |
Bytes 6-7 |
Red Optimal Duty Cycle (Transmitted in u8.8 format) Format = u8.8 |
Bytes 8-9 |
Green Optimal Duty Cycle (Transmitted in u8.8 format) Format = u8.8 |
Bytes 10-11 |
Blue Optimal Duty Cycle in (Transmitted in u8.8 format) Format = u8.8 |
Gets Ideal Duty Cycle for Current Target Color Point and the closest Duty Cycle Available. Sensor calibration Data should be set before using this command. |
Set WPC Calibration Data | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
LED Color 0 = Red 1 = Green 2 = Blue |
Bytes 1-2 |
Chromatic x coordinate in u1.15 format |
Bytes 3-4 |
Chromatic y coordinate in u1.15 format |
Bytes 5-8 |
Luminance Y coordinate |
Set WPC sensor calibration data through this command. WPC_Init() should complete successfully before invoking this command. |
Get WPC Calibration Data | |
---|---|
Read Parameters | |
Byte | Description |
Byte 0 |
LED Color 0 = Red 1 = Green 2 = Blue |
Return Parameters | |
Byte | Description |
Bytes 0-1 |
Chromatic x coordinate in u1.15 format |
Bytes 2-3 |
Chromatic y coordinate in u1.15 format |
Bytes 4-7 |
Luminance Y coordinate |
Bytes 8-11 |
Red Sensor Output |
Bytes 12-15 |
Green Sensor Output |
Bytes 16-19 |
Blue Sensor Output |
Bytes 20-21 |
Duty Cycle Format = u8.8 |
Gets WPC sensor calibration data through this command |
Get WPC Sensor Output | |
---|---|
Return Parameters | |
Byte | Description |
Bytes 0-3 |
Red |
Bytes 4-7 |
Green |
Bytes 8-11 |
Blue |
Returns Output of Integrating Sensor for Red, Blue and Green |
Set Maximum SSI Drive Level | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
Color 0 = SSI SPI/PWM designator for RED 1 = SSI SPI/PWM designator for GREEN 2 = SSI SPI/PWM designator for BLUE 3 = Sample1 for SPI systems. 4 = Sample2 C2 5 = SSI SPI Yellow/ IR for PWM systems. 6 = SSI CYAN for SPI SENSE for PWM systems 7 = SSI MAGENTA for SPI / Frequency for PWM systems 8 = SSI SPI designator for WHITE 9 = SSI SPI designator for Black 10 = SSI SPI designator for IR |
Bytes 1-2 |
Max Drive Level |
Set Maximum Drive Level |
Get Maximum SSI Drive Level | |
---|---|
Read Parameters | |
Byte | Description |
Byte 0 |
Color 0 = SSI SPI/PWM designator for RED 1 = SSI SPI/PWM designator for GREEN 2 = SSI SPI/PWM designator for BLUE 3 = Sample1 for SPI systems. 4 = Sample2 C2 5 = SSI SPI Yellow/ IR for PWM systems. 6 = SSI CYAN for SPI SENSE for PWM systems 7 = SSI MAGENTA for SPI / Frequency for PWM systems 8 = SSI SPI designator for WHITE 9 = SSI SPI designator for Black 10 = SSI SPI designator for IR |
Return Parameters | |
Byte | Description |
Bytes 0-1 |
Max Drive Level |
Get Maximum Drive Level |
Set SSI Duty Cycle Index | |
---|---|
Write Parameters | |
Byte | Description |
Bytes 0-1 |
Index |
Select Duty Cycle index for SSI |
Get SSI Duty Cycle Index | |
---|---|
Return Parameters | |
Byte | Description |
Bytes 0-1 |
Number Of Duty Cycles |
Bytes 2-3 |
Current Duty Cycle Index |
Bytes 4-5 |
Current Red Duty Cycle Format = u8.8 |
Bytes 6-7 |
Current Green Duty Cycle Format = u8.8 |
Bytes 8-9 |
Current Blue Duty Cycle Format = u8.8 |
Bytes 10-11 |
Current Yellow Duty Cycle Format = u8.8 |
Bytes 12-13 |
Current Cyan Duty Cycle Format = u8.8 |
Bytes 14-15 |
Current Magenta Duty Cycle Format = u8.8 |
Bytes 16-17 |
Current White Duty Cycle Format = u8.8 |
Get Details of selected Duty Cycles and number of duty cycles available in current system look |
Set Enable XPR Calibration Mode | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
1 - Calibration mode enabled |
This command sets the system in bypass mode. Setting the system in bypass mode disables any image processing to establish one to one correspondence between pixels on input source image and display image. Desirable for seeing clear splits of XPR subframes. There is no exit from calibration mode. Please restart the system. |
Get Enable XPR Calibration Mode | |
---|---|
Data returned is in the same format as the Write Parameters. | |
This command gets the state of XPR calibration mode. Whether enabled or not. |
Set WPC Calibration Structure Override | |
---|---|
Write Parameters | |
Byte | Description |
Byte 0 |
LED Color 0 = Red 1 = Green 2 = Blue |
Bytes 1-2 |
Chromatic x coordinate in u1.15 format |
Bytes 3-4 |
Chromatic y coordinate in u1.15 format |
Bytes 5-8 |
Luminance Y coordinate |
Bytes 9-12 |
Red Sensor Output |
Bytes 13-16 |
Green Sensor Output |
Bytes 17-20 |
Blue Sensor Output |
Bytes 21-22 |
Duty Cycle Format = u8.8 |
Set the entire WPC sensor calibration data structure through this command. WPC_Init() must complete successfully before invoking this command. |