JAJS392N July 2001 – January 2025 TPS793
PRODUCTION DATA
The legacy chip of TPS793 PMOS-pass transistor has a built-in back diode that conducts reverse current when the input voltage drops below the output voltage (for example, during power down). Current is conducted from the output to the input and is not internally limited. If extended reverse voltage operation is anticipated, external limiting to 5% of the rated output current is recommended.
The new chip of TPS793, as with most modern LDOs, excessive reverse current can damage this device.
Reverse current flows through the body diode on the pass element instead of the normal conducting channel. At high magnitudes, this current flow degrades the long-term reliability of the device as a result of one of the following conditions:
Conditions where reverse current can occur are outlined in this section, all of which can exceed the absolute maximum rating of VOUT > VIN + 0.3 V:
If reverse current flow is expected in the application, external protection must be used to protect the device. Figure 6-6 shows one approach of protecting the device.
Figure 6-6 Example Circuit for Reverse Current Protection
Using a Schottky Diode