JAJSHT5E February 2019 – December 2024 CC3135MOD
PRODUCTION DATA
The 3-wire UART topology requires only the following lines (see Figure 7-12).
Figure 7-12 3-Wire UART TopologyUsing 3-wire topology requires one of the following conditions to be met:
Because there is no full flow control, the host cannot stop the SimpleLink device to send its data; thus, the following parameters must be carefully considered: