JAJSI70C May 2008 – November 2019 DAC9881
PRODUCTION DATA.
The inherent architecture of the DAC9881, which consists of an R-2R architecture, enables great performance in regards to noise and accuracy, but at a cost of large glitch area. Glitch area, also known as glitch impulse area, is defined as the area associated with the overshoot or undershoot created by a code transition, and is generally quantified in Volt-seconds. Different code-to-code transitions produce different levels of glitch impulses. DACs with R-2R architectures produce large glitches during major-carry transitions.
There are two methods that can be used to reduce this glitch area:
Figure 72. Simplified Sample and Hold Circuit