JAJSPM1C March 2011 – November 2023 TPS40170
PRODUCTION DATA
The TPS40170 provides an indication that the output voltage of the converter is within the specified limits of the regulation as measured at the FB pin. The PGOOD pin is an open-drain signal and pulls low when any condition exists that can indicate that the output of the supply can be out of regulation. These conditions include:
Figure 6-17 shows a situation where no fault is detected during the start-up, (the normal PGOOD situation). The figure shows that PGOOD goes high tPGD (20 µs, typical) after all the conditions (listed above) are met.
Figure 6-17 PGOOD SignalWhen there is no power to the device, PGOOD is not able to pull close to GND if an auxiliary supply is used for the power good indication. In this case, a built-in resistor connected from drain to gate on the PGOOD pulldown device allows the PGOOD pin to operate like as a diode to GND.