JAJSPM1C March 2011 – November 2023 TPS40170
PRODUCTION DATA
The TPS40170 has both fixed and programmable input undervoltage lockout (UVLO). In order for the device to turn ON, all of the following conditions must be met:
In order for the device to turn OFF, any one of the following conditions must be met:
Programming the input UVLO can be accomplished using the UVLO pin. A resistor divider from the input voltage (VIN pin) to GND sets the UVLO level. After the input voltage reaches a value that meets the VUVLO level at the UVLO pin, then a small hysteresis current, IUVLO at the UVLO pin is switched in. The programmable UVLO function is shown in Figure 6-2.
Figure 6-2 UVLO Functional Block Schematic