JAJSRS4C October 2023 – February 2025 MSPM0C1103 , MSPM0C1104
PRODUCTION DATA
The event manager transfers digital events from one entity (for example, a peripheral) to another (for example, a second peripheral, the DMA or the CPU). The event manager implements event transfer through a defined set of event publishers (generators) and subscribers (receivers) that are interconnected through an event fabric containing a combination of static and programmable routes.
Events that are transferred by the event manager include:
For more details, see the Event chapter of the MSPM0 C-Series 24MHz Microcontrollers Technical Reference Manual.
| CHANID | Generic Route Channel Selection | Channel Type |
|---|---|---|
| 0 | No generic event channel selected | N/A |
| 1 | Generic event channel 1 selected | 1 : 1 |