JAJSSX2 February 2025 LMG3650R025
ADVANCE INFORMATION
The layout of the LMG365xR025 is critical to its performance and functionality. Because the half-bridge configuration is typically used with these GaN devices, layout recommendations are considered with this configuration. A four-layer or higher layer count board is required to reduce the parasitic inductances of the layout to achieve suitable performance. Critical layout guidelines are summarized below, and more details are further elaborated in the following sections.