JAJSVS7 November 2024 BQ21088
PRODUCTION DATA
The pushbutton function implemented through TS/MR pin has three main functions. First, it serves as a means to wake the device from ultra-low power modes like Factory mode. Second, it serves as a short button press detector, sending an interrupt to the host when the button driving the TSMR pin has been pressed for a Wake1, Wake2 or long press durations. This allows the implementation of different functions in the end application such as menu selection and control. Finallyit serves as a mean to get device into , Shutdown mode,or reset the system by performing a power cycle (shut down SYS and automatically powering it back on) after detecting a long button press. The timing for the short and long button press duration is programmable through I2C for added flexibility and allows system designers to customize the end user experience of a specific application. Note that if a specific timer duration is changed through I2C while that timer is active and has not expired, the new programmed value will be ignored until the timer expires and/or is reset by /MR.