JAJSVY4 December 2024 LMX2624-SP
ADVANCE INFORMATION
The frequency doubler is used to produce an output frequency that is twice the VCO frequency at RFOUTA and at RFOUTB based on OUTMUX2, OUTMUX1 and OUTMUX0 settings. When the VCO frequency is doubled, the fundamental (non-doubled) VCO frequency does leak to the output and this is the sub-harmonic (0.5X). To minimize these sub-harmonics, there is tunable filter that tracks the output frequency and filters out this sub-harmonic as well as other undesired harmonics (1.5X, 2X, 3X, ...). The calibration for this tunable filter is automatically triggered whenever the VCO calibration is done.