JAJSVY4 December 2024 LMX2624-SP
ADVANCE INFORMATION
Double buffering—also known as "shadow registers"—allows the user to program multiple registers without having them actually take effect. Then when the R0 register is programmed, then these registers take effect. This is especially useful if one wants to change frequencies quickly and multiple register writes are required. When DBLBUF_EN = 1, the double buffering is enabled for the registers related to VCO, Doubler, PLL, Output MUX and Channel Divider. More details on the registers are available in Register map section.
For the no assist method, just set VCO_SEL=7 and this is done. For partial assist, the VCO calibration speed can be improved by changing the VCO_SEL bit according to the frequency. Note that the frequency is not the actual VCO core range, but favors choosing the VCO. This is not only optimal for VCO calibration speed, but required for reliable locking.
| fVCO | VCO CORE (MIN) |
|---|---|
| 7500 - 8600MHz | VCO1 |
| 8600 - 9900MHz | VCO2 |
| 9900 - 10800MHz | VCO3 |
| 10800 -11900MHz | VCO4 |
| 11900 - 13000MHz | VCO5 |
| 13000 - 14000MHz | VCO6 |
| 14000 - 15000MHz | VCO7 |
For fastest calibration time, use the minimum VCO core as recommended in the previous table. The following table shows typical VCO calibration times for this choice in bold as well as showing how long the calibration time is increased if a higher than necessary VCO core is chosen. Realize that these calibration times are specific to these fOSC and fPD conditions specified and at the boundary of two cores, sometimes the calibration time can be increased.
| fVCO | VCO_SEL#OL_ENF_TDS_RDC | ||||||
|---|---|---|---|---|---|---|---|
| VCO7 | VCO6 | VCO5 | VCO4 | VCO3 | VCO2 | VCO1 | |
| 8.1 GHz | 650 | 614 | 620 | 376 | 256 | 243 | 191 |
| 9.3 GHz | 606 | 589 | 587 | 335 | 196 | 177 | Invalid |
| 10.4 GHz | 598 | 579 | 570 | 338 | 177 | Invalid | |
| 11.4 GHz | 543 | 540 | 530 | 284 | Invalid | ||
| 12.5 GHz | 396 | 346 | 300 | Invalid | |||
| 13.6 GHz | 262 | 218 | Invalid | ||||
| 14.7 GHz | 164 | Invalid | |||||
| fVCO | VCO_SEL(1) | ||||||
|---|---|---|---|---|---|---|---|
| VCO7 | VCO6 | VCO5 | VCO4 | VCO3 | VCO2 | VCO1 | |
| 8.1 GHz | 854 | 828 | 822 | 579 | 451 | 437 | 393 |
| 9.3 GHz | 819 | 800 | 794 | 551 | 401 | 380 | Invalid |
| 10.4 GHz | 808 | 786 | 781 | 551 | 388 | Invalid | |
| 11.4 GHz | 767 | 745 | 743 | 494 | Invalid | ||
| 12.5 GHz | 603 | 560 | 513 | Invalid | |||
| 13.6 GHz | 469 | 426 | Invalid | ||||
| 14.7 GHz | 385 | Invalid | |||||