JAJU833 November 2021 AWR2944 , IWR2944
The performance of the AWR2944 corner radar functionality was tested using the demonstration available in the TI Resource Explorer in the Automotive Toolbox: lab01027. The AWR2944BOOST EVM was used for the tests. Figure 3-3 illustrates a test setup scenario. AWR2944EVM is mounted on the rear end of the mid-size car