JAJU833 November 2021 AWR2944 , IWR2944
This reference design uses Doppler division multiple access (DDMA) processing where most of processing is done on the HWA and some intermediate tasks are offloaded to the DSP.
| PARAMETER | SPECIFICATIONS | DETAILS |
|---|---|---|
| Maximum range (m) | 253 | This is the maximum range supported by the chirp configuration shown in Table 2-1. The maximum detectable range for a given object depends on the Radar cross section (RCS) of the object |
| Range resolution (m) | 1.3 | The theoretical achievable resolution by AWR2944 is 3.75 cm based on 4 GHz bandwidth |
| Maximum velocity (kmph) | ±143 | This is the native maximum velocity obtained after velocity disambiguation in DDMA. This specification can be improved by either using the range-rate in the tracker or higher-level algorithms |
| Velocity resolution (kmph) | 0.37 | This parameter represents the capability of the radar sensor to distinguish between two or more objects at the same range but moving with different velocities |
| Azimuth angular resolution (Deg) | 9.5 | This is the native azimuth angular resolution based on the virtual array aperture |