SBAA661 February 2025 LMX1205
Sometimes, one is stuck with a low input clock frequency, which is not designed for PLLs. In this case, if choosing a buffer strategically, then the buffer can improve the PLL phase noise. The Texas Instruments LMK1C1102 CMOS buffer has excellent noise floor and is very good at squaring up signals. Sine to Square Wave Conversion using Clock Buffers shows how this buffer can be used to improve the phase noise of the LMX2820, even for signal levels at the maximum allowable input power of +10dBm. This is very true for 10MHz and still true to just a small extent at even 100MHz input frequency.