SBAU269C October 2016 – August 2021 ADS8900B
The register map configuration tool allows the user to view and modify the registers of the ADS8900. This configuration can be selected by clicking on the Register Map Config radio button on the Pages section of the left pane shown in Figure 6-4. At power up, the values on this page correspond to the reset values of the device registers. The register values can be edited by double clicking the corresponding value field. If interface mode settings are affected by the change in register values, this change is reflected on the left pane immediately. The impact of changes in the register value reflect on the ADS8900 device based on the Update Mode selection as described in Section 6.1.
Figure 6-4 Register Map ConfigurationSection 6.3 through Section 6.6 describe the data collection and analysis features of the ADS8900EVM-PDK GUI.