SBOA564 December 2022 TRF0206-SP
The purpose of this study was to characterize the effect of heavy-ion irradiation on the single-event effect (SEE) performance of the TRF0206-SP 6.5-GHz, Low Noise, Low Power, Fully-Differential Amplifier. Extensive SEE testing with heavy-ions having LETEFF from 9.75 to 82.1 MeV-cm2/mg were conducted with heavy-ion fluences ranging from 106 to 107 ions/cm2 per run. The SEE results demonstrated that the TRF0206-SP is SEL-free up to LETEFF = 82.1 MeV-cm2/mg. Also the SET cross sections are discussed under static input conditions. CREME96-based worst-week event-rate calculations for LEO(ISS) and GEO orbits clearly demonstrate the robustness of the TRF0206-SP in two harshly conservative space environments.