SLAU857A May 2021 – July 2021 MSP430FR2476 , MSP430FR2512 , MSP430FR2522 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR2672 , MSP430FR2673 , MSP430FR2675 , MSP430FR2676
Software development for a capacitive touch application is complicated and requires software tools such as GUI and IDE. The development process includes setting parameters and function development. Therefore, before reading this chapter, read Section 3.3 and Section 6 to understand the entire capacitive touch development chain, and to be familiar with the basic operations of the GUI and IDE. For the information on the MSP430 MCU itself, refer to the MSP430™ MCUs Development Guide Book.
Capacitive touch software development can be roughly divided into five parts as shown in Figure 5-1. From the perspective of development time, software tuning takes the longest time. The following sections describe these development phases.
Figure 5-1 Software Design Process