Use the following steps to verify
battery charging in bypass mode.
- Make sure the steps in Section 4.1.1 and Section 4.1.2 have been followed.
- Set PS1 to 4.1 V. Load #1 can be
kept at 4.0 V.
- Make sure the "Enable Charge" box is not selected. Then, click
"Enable Bypass Mode".
- Click Enable Charge.
After enabling charge, the output current flowing into Load #1 is approximately
equal to the input current flowing out of PS1.
- Change the charge current:
By increasing the input voltage, the output
current increases together with the input current. The output current is always
approximately equal to the input current.
- To stop charging, deselect the
Enable Charge box. The input current and the output current both fall
to zero.