SLUUCU7 November 2023 BQ25960H
Out of the box, the BQ25960HEVM is configured to evaluate the performance of the BQ25960H only. If the BQ25611D must also be evaluated, then the user needs to populate R29 and R32, as shown in the schematic in Figure 6-3.
A typical use case is for the BQ25611D buck charger (U4) to perform low current pre-charge and charge termination, while one or both of the BQ25960H switched cap chargers (U1 and U2) perform high current fast charging to achieve the highest possible efficiency.
Use the following steps to charge with the BQ25611D. The I2C address for U4 is 0x6B.