Use the following steps to verify
battery charging in switched cap mode.
- Make sure the steps in Section 4.1.1 and Section 4.1.2 have been followed.
- Check the "CHG_CONFIG_1 box, and then click Enable Charge. After
enabling charge, the output current flowing into Load #1 is about 2x the input
current flowing out of PS1.
- Change the charge current:
By increasing the input voltage, the output
current increases together with the input current. The output current is always
about 2x the input current. - To stop charging, deselect the Enable
Charge box. The input current and the output current both fall to
zero.