SNVAA94 November 2023 LM5113-Q1 , LMG1205 , LMG1210
The LMG1210 uses a different method to prevent bootstrap overcharge. Like LMG1205, LMG1210 uses a switch in series with the bootstrap diode path. However, LMG1210 switches on when the low-side output (LO) is high, unlike LMG1205, which switches only with overvoltage on Cboot.
Bootstrap overcharging happens during the dead time because of the GaN FET third-quadrant behavior that creates large negative voltages on HS. Blocking the bootstrap diode during the dead time on every cycle prevents any possibility of overcharging. When LO is high, the dead time must be over. So, attaching the bootstrap switch state to LO consistently keeps the switch in the correct state. Figure 8-2 shows how conduction is blocked during the HS undershoot event and overcharging is prevented.
Figure 8-3 compares the same system with and without the series switch. The system behaves correctly with the switch—where the bootstrap capacitor charges when LO is high and reaches a steady state of approximately 4.4 V. This same system overcharges without the switch past 6 V and only charges during the dead time.
One benefit of avoiding dead-time conduction is the reduction of reverse recovery of the bootstrap diode. When the bootstrap diode is permitted to conduct before HS rises, the diode builds up a significant current. The bootstrap diode has a reverse recovery event when HO is turned on and HS rises. Reference Figure 8-3, where there is nearly 1 A of reverse recovery current, as opposed to the circuit with the switch, which shows a nominal reverse current. Preventing reverse recovery events is another benefit of this active switching technique.
A downside to this active switch method is that the method does not allow productive overcharging. Therefore, the high-side GaN FET gate voltage is always VDD minus a diode drop. A lower gate voltage means the high-side GaN FET has a higher resistance and experiences more conduction losses.
The active switch method does not rely on a fixed threshold voltage and has no response time issue like the overvoltage method. Additionally, the active switch is better for supporting both 5 V and 6 V gate GaN FETs because the switch lacks a fixed threshold.