The baseboard configuration is used for to interface the controlSOM directly to a
compatible baseboard or docking station. Power is provided to the controlSOM through the
baseboard. An emulation debug-probe such as the XDS110ISO-EVM is required to provide debug
connectivity to the MCU. The XDS110 debug-probe and baseboard are sold separately.
In this configuration, Code Composer Studio
Theia connects to the controlSOM via JTAG and enables software development. The XDS110
debug-probe also enumerates a virtual COM port (VCP) for communication with the MCU via
UART.
Follow the steps in the baseboard user's
guide to enable this configuration.
- The following equipment is required:
- AM261x controlSOM
(AM261-SOM-EVM)
- C2000, Sitara controlSOM compatible
base board
- XDS110 isolated debug probe
(XDS110ISO-EVM)
- One USB Type-C cable
- Verify the switch settings are correct on
each EVM.
- AM261-SOM-EVM:
- Use SW1 to select the desired
boot mode (Section 2.7).
- Use S1, S2, S4 to select the
desired ADC voltage reference mode (if applicable for the application) (Section 2.9.7).
- XDS110ISO-EVM:
- S1 selects JTAG mode; set to JTAG
mode.
- S2 enables UART, SPI connection;
set to ON mode
- Set up the base board as per the user's
guide instructions.
- Attach the AM261x ControlSOM to the
baseboard.
- Make sure the controlSOM is correctly
oriented. The J1 header on the controlSOM connects with the J1 header on the
baseboard.
- Connect the XDS110ISO-EVM into the XDS
Debug Header (J4) of the controlSOM.
- Connect the USB cable into connector J5
on the XDS110 isolated debug probe. The XDS110 isolated probe and the controlSOM are
powered on
- Provide power to the base board as per
the user's guide instructions.
- Verify the power status LEDs (D5, D6, D7)
on the controlSOM are turned on.
- The controlSOM is ready for use. Follow
the steps in Section 3 to get started on developing software.