SPRACS8 May   2022 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

 

  1.   Trademarks
  2. 1Introduction
  3. 2Hardware Connection
  4. 3C2000 I2C Source Code
    1. 3.1 I2CHandle Description
    2. 3.2 I2CBusScan
    3. 3.3 I2C_MasterTransmitter
    4. 3.4 I2C_MasterReceiver
  5. 4EEPROM Byte Write
  6. 5EEPROM Byte Read
  7. 6EEPROM Word Write
  8. 7EEPROM Word Read
  9. 8EEPROM Paged Write
  10. 9EEPROM Paged Read

I2C_MasterReceiver

Function name: I2C_MasterReceiver(I2CA_BASE, struct I2CHandle *pI2C_Params)

Description: This function can be used to receive 'N' number of bytes defined in pI2C_Params. This function can also be used to perform the following EEPROM read operations.

  1. EEPROM byte read

    Set Number of bytes to be read (EEPROM.NumOfDataBytes = 1)

  2. EEPROM word read

    Set Number of bytes to be read (EEPROM.NumOfDataBytes = 2) - Two bytes make a word

  3. EEPROM Paged read

    Set Number of bytes to be read (EEPROM.NumOfDataBytes = 'N') . There is no page size restriction for paged read.

    Below setting applies to all the above EEPROM read operations

    Set EEPROM.NumOfAddrBytes = 2, because high address byte and low address byte needs to be transmitted

Arguments:

base : base is the base address of the I2C instance used

pI2C_Params : Pointer to I2C address handle of the slave

Return:Status of I2C transaction