SPRACV2 November 2020 AWR1843 , AWR2243
Customers may choose to calibrate the TX phase shifters (e.g. for better accuracy) using corner reflectors in the factory. This procedure is an alternative to using the devices’ self-calibration of TX phase shift using RF INIT. An example measurement procedure is as follows.
If deriving the phase shifter calibration values from corner reflector measurements in customer factory:
The arrays Factory Measured Phase Shift ArrayCornerReflector,TXm (0 to 63) collected at factory temperature are necessary for restoring back to the device (explained later in this document). Example values for the Measured Phase Shift Arrays of Equation 2: [0, 5, 11, … 356] degrees, corresponding to [0, 5.625, 11.25, … 354.375] degree phase shifter settings. These correspond to INL error values of [0, 0.625, 0.25, …, –1.625] degree, i.e. the deviation from ideal expectations. Here, INL error refers to Integrated Non Linearity error.
Here are some APIs relevant for achieving this:
| Device 1 | Device 2 | ||||||
|---|---|---|---|---|---|---|---|
| Chirp Index | Enable TX1 | Enable TX2 | Enable TX3 | Enable TX1 | Enable TX2 | Enable TX3 | Phase Shift Index (common to all TXs) |
| 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 (0o) |
| 1 | 1 | 0 | 0 | 0 | 0 | 0 | 1 (5.625o) |
| 2 | 1 | 0 | 0 | 0 | 0 | 0 | 2 (11.25o) |
| : | 1 | 0 | 0 | 0 | 0 | 0 | : |
| 63 | 1 | 0 | 0 | 0 | 0 | 0 | 63 (354.375o) |
| 64+0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 (0o) |
| 64+1 | 0 | 1 | 0 | 0 | 0 | 0 | 1 (5.625o) |
| 64+2 | 0 | 1 | 0 | 0 | 0 | 0 | 2 (11.25o) |
| 64+: | 0 | 1 | 0 | 0 | 0 | 0 | : |
| 64+63 | 0 | 1 | 0 | 0 | 0 | 0 | 63 (354.375o) |
| 2*64+0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 (0o) |
| 2*64+1 | 0 | 0 | 1 | 0 | 0 | 0 | 1 (5.625o) |
| 2*64+2 | 0 | 0 | 1 | 0 | 0 | 0 | 2 (11.25o) |
| 2*64+: | 0 | 0 | 1 | 0 | 0 | 0 | : |
| 2*64+63 | 0 | 0 | 1 | 0 | 0 | 0 | 63 (354.375o) |
| 3*64+0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 (0o) |
| 3*64+1 | 0 | 0 | 0 | 1 | 0 | 0 | 1 (5.625o) |
| 3*64+2 | 0 | 0 | 0 | 1 | 0 | 0 | 2 (11.25o) |
| 3*64+: | 0 | 0 | 0 | 1 | 0 | 0 | : |
| 3*64+63 | 0 | 0 | 0 | 1 | 0 | 0 | 63 (354.375o) |
| 4*64+0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 (0o) |
| 4*64+1 | 0 | 0 | 0 | 0 | 1 | 0 | 1 (5.625o) |
| 4*64+2 | 0 | 0 | 0 | 0 | 1 | 0 | 2 (11.25o) |
| 4*64+: | 0 | 0 | 0 | 0 | 1 | 0 | : |
| 4*64+63 | 0 | 0 | 0 | 0 | 1 | 0 | 63 (354.375o) |
| 5*64+0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 (0o) |
| 5*64+1 | 0 | 0 | 0 | 0 | 0 | 1 | 1 (5.625o) |
| 5*64+2 | 0 | 0 | 0 | 0 | 0 | 1 | 2 (11.25o) |
| 5*64+: | 0 | 0 | 0 | 0 | 0 | 1 | : |
| 5*64+63 | 0 | 0 | 0 | 0 | 0 | 1 | 63 (354.375o) |
At 25C, the measured phase shift array from corner reflector-based experiments from TX1 of typical AWR2243 device (nominal process) is tabulated in Table 8 in the Appendix section. The same in the form of phase shifter INL plot at 25C is represented in Figure 3-1(b). These have been obtained in TI lab evaluation of few nominal process based devices. They provide representative information and can be used for example in initial sensor development. There can be some amount of process variation in the INL but the trend is expected to be roughly similar (based on evaluation of DoE devices in TI lab).
For post-calibration phase shifter accuracy with 25C factory calibration using corner reflector, refer to Figure 5(b).