SPRAD96B November 2023 – January 2024 AM62P , AM62P-Q1
The middle priority interfaces and the power distribution planes and pours would be routed next after the SerDes and DDR interfaces. It is strongly encouraged to complete all SerDes and DDR routing before continuing with other interfaces. The power distribution planes and pours and all of the decoupling must be placed before PCB simulations are executed for the SerDes and DDR routes, as these can influence the return currents for the high-speed interfaces. The highest speed source-synchronous interfaces, such as RGMII and QSPI, may also require simulation, so these may also need to be completed at this time.
Special care is needed for the 1-uF output capacitors connected to the CAP_VDDS* BGA pins on the AM62Px device. These capacitors should be placed as close to the pin as possible and a low inductance path should be present between the CAP_VDDS BGA pin and the supply pad on the capacitor.
This placement can be improved if the capacitors can be placed directly under the SoC. The decoupling capacitors for the VDD_CORE and VDDS_DDR supplies should also receive the same priority as those on the CAP_VDDS* pins and should be placed under the socket, with minimum inductance connections to the respective BGA pins on the AM62Px device.