SPRUHW1A June 2014 – October 2021 TMS320F28052-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28054-Q1 , TMS320F28054M , TMS320F28054M-Q1
In order for the 2805xM devices to use InstaSPIN, the volatile memory area used by the libraries in ROM must be reserved. The following code listing of the RAM area shows that L0 RAM should not be used. To avoid conflicts between user's memory and library used memory, variables declared by the user must not use this memory range.