SPRUIZ4B May   2021  – June 2022

 

  1.   F280039C controlCARD Information Guide
  2.   Trademarks
  3. 1Introduction
  4. 2Hardware Quick Setup Guide
  5. 3Errata
    1. 3.1 Warnings, Notes, and Errata
    2. 3.2 Warnings About Specific controlCARD Revisions
  6. 4Getting Familiar With the controlCARD
    1. 4.1 F280039C controlCARD Features
    2. 4.2 Assumed Operating Conditions
    3. 4.3 Using the controlCARD
    4. 4.4 Experimentation Software
  7. 5Special Notes
    1. 5.1 XDS110 Emulator and SCI (UART) Connectivity
    2. 5.2 Clocking Methodology
    3. 5.3 Evaluation of the Analog-to-Digital Converters (ADCs)
  8. 6Hardware References
  9. 7Revision History

Hardware Quick Setup Guide

The controlCARD can be completely powered and operated from the USB-C connector. In this stand-alone mode the on-board isolated power supply will provide power to the F280039C device; no additional hardware is required. Optionally, an external 5-V supply can be provided to power the F280039C device. For a detailed explanation of the hardware configuration, see Section 4.3.

WARNING:

When the controlCARD is used in a high-voltage setup, it is the user’s responsibility to confirm that the voltages and isolation requirements are identified and understood prior to energizing the board or simulation. When energized, the controlCARD or components connected to the controlCARD should not be touched. Furthermore, the capacitor C7:A should be removed to minimize the possibility of leakage current flowing across the isolation barrier of the controlCARD.

Configuration 1: Stand-alone

  1. Connect a USB-C cable to J1:A.
  2. Connect the other end of the USB cable to a USB2.0/USB3.x port.
  3. LED1:A and D3 on the controlCARD will illuminate.

Configuration 2: External 5-V supply

  1. Insert the TMDSCNCD280039C controlCARD into a TMDSHSECDOCK, or other compatible docking station.
  2. Connect a USB-B "mini" connector to J17 on the TMDSHSECDOCK.
  3. Flip S1 to the "USB-ON" position. The controlCARD will automatically switch to the external 5-V supply.
  4. LED1:A and D3 on the controlCARD will illuminate.
Note:

The TMDSCNCD280039C controlCARD automatically switches to the external 5-V supply when present. No additional configuration is required.