SPRUJ40C may   2022  – may 2023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1EVM Revisions and Assembly Variants
  5. 2System Description
    1. 2.1 Key Features
      1. 2.1.1 Thermal Compliance
      2. 2.1.2 Processor
      3. 2.1.3 Power Supply
      4. 2.1.4 Memory
      5. 2.1.5 JTAG/Emulator
      6. 2.1.6 Supported Interfaces and Peripherals
      7. 2.1.7 Expansion Connectors/Headers to Support Application Specific Add‐On Boards
    2. 2.2 Functional Block Diagram (SK-AM62 and SK-AM62B)
    3. 2.3 Functional Block Diagram (SK-AM62-P1 and SK-AM62B-P1)
    4. 2.4 AM62x SKEVM Interface Mapping
    5. 2.5 Power ON/OFF Procedures
      1. 2.5.1 Power-On Procedure
      2. 2.5.2 Power-Off Procedure
      3. 2.5.3 Power Test Points
    6. 2.6 Peripheral and Major Component Description
      1. 2.6.1  Clocking
        1. 2.6.1.1 Peripheral Ref Clock
      2. 2.6.2  Reset
      3. 2.6.3  OLDI Display Interface
      4. 2.6.4  CSI Interface
      5. 2.6.5  Audio Codec Interface
      6. 2.6.6  HDMI Display Interface
      7. 2.6.7  JTAG Interface
      8. 2.6.8  Test Automation Header
      9. 2.6.9  UART Interface
      10. 2.6.10 USB Interface
        1. 2.6.10.1 USB 2.0 Type A Interface
        2. 2.6.10.2 USB 2.0 Type C Interface
      11. 2.6.11 Memory Interfaces
        1. 2.6.11.1 DDR4 Interface
        2. 2.6.11.2 OSPI Interface
        3. 2.6.11.3 MMC Interfaces
          1. 2.6.11.3.1 MMC0 - eMMC Interface
          2. 2.6.11.3.2 MMC1 - Micro SD Interface
          3. 2.6.11.3.3 MMC2 - Wilink Interface
        4. 2.6.11.4 EEPROM
      12. 2.6.12 Ethernet Interface
        1. 2.6.12.1 CPSW Ethernet PHY 2 Default Configuration
        2. 2.6.12.2 CPSW Ethernet PHY 1 Default Configuration
      13. 2.6.13 GPIO Port Expander
      14. 2.6.14 GPIO Mapping
      15. 2.6.15 Power
        1. 2.6.15.1 Power Requirements
        2. 2.6.15.2 Power Input
        3. 2.6.15.3 Power Supply
        4. 2.6.15.4 Power Sequencing
        5. 2.6.15.5 AM62x SoC Power
        6. 2.6.15.6 Current Monitoring
      16. 2.6.16 AM62x SKEVM User Setup/Configuration
        1. 2.6.16.1 EVM DIP Switches
        2. 2.6.16.2 Boot Modes
        3. 2.6.16.3 User Test LEDs
      17. 2.6.17 Expansion Headers
        1. 2.6.17.1 PRU Connector
        2. 2.6.17.2 User Expansion Connector
        3. 2.6.17.3 MCU Connector
      18. 2.6.18 Interrupt
      19. 2.6.19 I2C Address Mapping
  6. 3Known Issues and Modifications
    1. 3.1  Issue 1 - HDMI/DSS Incorrect Colors on E1
    2. 3.2  Issue 2 - J9 and J10 Header Alignment on E1
    3. 3.3  Issue 3 - USB Boot descoped on E1
    4. 3.4  Issue 4 - OLDI Connector Orientation and Pinout
    5. 3.5  Issue 5 - Bluetooth descoped on E2 EVMs
    6. 3.6  Issue 6 - Ethernet PHY CLK Skew Default Strapping Changes
    7. 3.7  Issue 7 - TEST_POWERDOWN changes
    8. 3.8  Issue 8 - MMC1_SDCD spurious interrupts
    9. 3.9  Issue 9 - PD Controller I2C2 IRQ Not Pinned Out
    10. 3.10 Issue 10 - INA Current Monitor Adress Changes
    11. 3.11 Issue 11 - Test Automation I2C Buffer Changes
  7.   Regulatory Compliance
  8.   Revision History

Boot Modes

The boot mode for the SK EVM board is defined by two banks of switches SW1 and SW2 or by the I2C buffer connected to the Test automation connector. This allows for AM62x SoC Boot mode control by either the user (DIP Switch Control) or by the Test Automation connector.

All the bits of switch (SW1 and SW2) have week pull down resistor and a strong pull up resistor as shown in below picture. Note that OFF setting provides a low logic level (‘0’) and an ON setting provides a high logic level (‘1’).
Note: The boot mode orientation has changed between E1 and future revisions. Please follow board silkscreen.
GUID-20230425-SS0I-3MWJ-5S0F-K2QGMZQJ6XWF-low.png Figure 2-17 Bootmode Switch Configuration for SD Boot (From E2)
GUID-05AF1FC2-8ED7-44B1-89E4-9A0B1F167531-low.png Figure 2-18 Bootmode Switch Configuration for SD Boot (E1)

The boot mode pins of the SoC have associated alternate functions during normal operation. Hence isolation is provided using Buffer IC’s to cater for alternate pin functionality. The output of the buffer is connected to the bootmode pins on the AM62x and the output is enabled when the bootmode is needed during a reset cycle. The input to the buffer is connected to the DIP switch circuit and to the output of an I2C buffer set by the test automation circuit. If the test automation circuit is going to control the bootmode, all the switches will manually be set to the OFF position. The bootmode buffer should be powered by an always ON power supply to ensure that the bootmode remains present even if the SoC power is cycled.

Switch SW1 and SW2 bits [15:0] are used to set the SoC Boot mode.

The switch map to the boot mode functions is provided in the tables below.

Table 2-17 BOOT-MODE Pin Mapping
Bit 15 Bit 14 Bit 13 Bit 12 Bit 11 Bit 10 Bit 9 Bit 8 Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
Reserved Reserved Backup Boot Mode Configuration Backup Boot Mode Primary Boot Mode Configuration Primary Boot Mode PLL Configuration
  • BOOT-MODE [0:2] – Denote system clock frequency for PLL configuration. By default, this bits are set for 25 MHz.

Table 2-18 gives details ON PLL reference clock selection.

Table 2-18 PLL Reference Clock Selection BOOTMODE [2:0]
Bit 2 Bit 1 Bit 0 PLL REF CLK (MHz)
OFF OFF OFF RSVD
OFF OFF ON RSVD
OFF ON OFF 24
OFF ON ON 25
ON OFF OFF 26
ON OFF ON RSVD
ON ON OFF RSVD
ON ON ON RSVD
  • BOOT-MODE [3:6] – This provides primary boot mode configuration to select the requested boot mode after POR, that is, the peripheral/memory to boot from. Table 2-19 provides primary boot device selection details.
Table 2-19 Boot Device Selection BOOT-MODE [6:3]
Bit 6 Bit 5 Bit 4 Bit 3 Primary Boot Device Selected
OFF OFF OFF OFF Serial NAND
OFF OFF OFF ON OSPI
OFF OFF ON OFF QSPI
OFF OFF ON ON SPI
OFF ON OFF OFF Ethernet RGMII1
OFF ON OFF ON Ethernet RMII1
OFF ON ON OFF I2C
OFF ON ON ON UART
ON OFF OFF OFF MMC/SD card
ON OFF OFF ON eMMC
ON OFF ON OFF USB0
ON OFF ON ON GPMC NAND
ON ON OFF OFF GPMC NOR
ON ON OFF ON Rsvd
ON ON ON OFF xSPI
ON ON ON ON No boot/Dev Boot
  • BOOT-MODE [10:12] – Select the backup boot mode, that is, the peripheral/memory to boot from, if primary boot device failed.

Table 2-20 provides backup boot mode selection details.

Table 2-20 Backup Boot Mode Selection BOOT-MODE [12:10]
Bit 12 Bit 11 Bit 10 Backup Boot Device Selected
OFF OFF OFF None (No backup mode)
OFF OFF ON USB
OFF ON OFF Reserved
OFF ON ON UART
ON OFF OFF Ethernet
ON OFF ON MMC/SD
ON ON OFF SPI
ON ON ON I2C
  • BOOT-MODE [9:7] – These pins provide optional settings and are used in conjunction with the primary boot device selected.

Table 2-21 gives primary boot media configuration details.

Table 2-21 Primary Boot Media Configuration BOOT-MODE [9:7]
Bit 9 Bit 8 Bit 7 Boot Device
Reserved Read Mode 2 Read Mode 1 Serial NAND
Speed Iclk Csel OSPI
Reserved Iclk Csel QSPI
Reserved Mode Csel SPI
Clkout Delay Link stat Ethernet RGMII
Clkout Clk src Reserved Ethernet RMII
Bus Reset Reserved Addr I2C
Reserved Reserved UART
Port Reserved Fs/raw MMC/ SD card
Reserved voltage eMMC
Reserved Mode Lane swap USB0
Reserved GPMC NAND
Reserved GPMC NOR
Reserved Reserved
SFDP Read Cmd Mode xSPI
Reserved No/Dev No boot/Dev Boot
  • BOOT-MODE [13] – These pins provide optional settings and are used in conjunction with the backup boot device devices. Switch SW2.6 when ON sets 1 and sets 0 if OFF, see the device-specific TRM.
  • BOOT-MODE [14:15] – Reserved.

Table 2-22 provides backup boot media configuration options.

Table 2-22 Backup Boot Media Configuration BOOT-MODE [13]
Bit 13 Boot Device
Reserved None
Mode USB
Reserved Reserved
Reserved UART
IF Ethernet
Port MMC/SD
Reserved SPI
Reserved I2C