SPRZ412M December 2013 – March 2023 TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
ADC: DMA Read of Stale Result
0, A, B, C
The ADCINT flag can be set before the ADCRESULT value is latched (see the tLAT and tINT(LATE) columns in the ADC Timings tables of the TMS320F2837xD Dual-Core Real-Time Microcontrollers data sheet). The DMA can read the ADCRESULT value as soon as 3 cycles after the ADCINT trigger is set. As a result, the DMA could read a prior ADCRESULT value when the user expects the latest result if all of the following are true:
Only the DMA reads listed above could result in reads of stale data; the following non-DMA methods will always read the expected data:
Trigger two DMA channels from the ADCINT flag. The first channel acts as a dummy transaction. This will result in enough delay that the second channel will always read the fresh ADC result.