SPRZ412M December 2013 – March 2023 TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
Boot ROM: Using CPU1 Wait Boot or CPU2 Idle Mode
0, A, B, C
The PIE Initialize Vector Table function that is part of the CPU1 and CPU2 ROMs writes beyond the PIE vector table addresses, up to address 0x1080. If the DMA clock is enabled before a debugger reset and CPU1 goes to wait boot (or CPU2 goes to idle mode), then some DMA registers will be overwritten during the ROM PIE vector initialization.
None