SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The CMD_PROP_TX command transmits a packet with the format from Table 26-172. The parameters are as given in Table 26-168.
The packet transmission starts at the given start trigger, with a fixed delay. The modem first transmits the preamble and sync word as configured. The sync word to transmit is given in the syncWord field, in the LSBs if less than 32 bits are used. The word is transmitted in the bit order programmed in the radio.
If pktConf.bVarLen is 1, a length byte equal to the value of pktLen is sent next. After this, the content of the buffer pointed to by pPkt is sent. This buffer consists of the number of bytes given in pktLen. If an address byte as shown in Figure 26-9 is needed, it must be sent as the first payload byte.
If pktConf.bUseCrc is 1, a CRC is calculated and transmitted at the end. The number of CRC bits, polynomial, and initialization are as configured in the radio. The CRC is calculated over the length byte (if present) and over the entire contents of the buffer pointed to by pPkt.
If whitening is enabled, the optional length byte, the entire contents of the buffer pointed to by pPkt, and the CRC are subject to whitening. The whitening is done after the data is used for CRC calculation.