SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Get Local Name

Description

This function is responsible for querying the name of the local Bluetooth Device. This function returns zero on a successful execution and a negative value on all errors. A Bluetooth StackID must exist before attempting to call this function.

Parameters

It is not necessary to include parameters when using this command. A parameter will have no effect on the outcome of the Query.

Possible Return Values

  • (0) Successfully Queried Local Device Name
  • (-8) INVALID_STACK_ID_ERROR
  • (-4) FUNCTION_ERROR
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1) BTPS_ERROR_INVALID_PARAMETER
  • (-57) BTPS_ERROR_DEVICE_HCI_ERROR
  • (-65) BTPS_ERROR_INSUFFICIENT_BUFFER_SPACE

API Call

GAP_Query_Local_Device_Name(BluetoothStackID, 257, (char *)LocalName);

API Prototype

int BTPSAPI GAP_Query_Local_Device_Name(unsigned int BluetoothStackID, unsigned int NameBufferLength, char *NameBuffer);

Description of API

This function is responsible for querying (and reporting) the user friendly name of the local Bluetooth device. The final parameters to this function specify the buffer and buffer length ofthe buffer that is to receive the local device name. The NameBufferLength parameter should be at least (MAX_NAME_LENGTH+1) to hold the maximum allowable device name (plus asingle character to hold the NULL terminator). If this function is successful, this function returns zero, and the buffer that NameBuffer points to will be filled with a NULL terminatedASCII representation of the local device name. If this function returns a negative value, then the local device name was NOT able to be queried (error condition).