SWRU561A September 2020 – October 2020 WL1801MOD , WL1805MOD , WL1807MOD , WL1831 , WL1831MOD , WL1835MOD , WL1837MOD
In order to verify the connection, use the ping command. For example, if the Access Point IP address is 192.168.1.1, we will invoke the following command on the EVM:
ping 192.168.1.1
You should see the an output similar to the following:
PING 192.168.1.1 (192.168.1.1): 56 data bytes
64 bytes from 192.168.1.1: seq=0 ttl=64 time=1003.369 ms
64 bytes from 192.168.1.1: seq=1 ttl=64 time=2.526 ms
You can also invoke the command. This command will display the AP settings and verify the
connection iw wlan0 link
.