DLPU082C August 2021 – March 2024 DLPC7540
63 horizontal and 32 vertical control points define a 63×32 map on the input image. Half the control points must be in the left half of image and half in the right half of image. From a total of 2016 control points, 1008 control points need to be in each half of the image when the image is divided vertically in two halves from the middle of the horizontal resolution.
While declaring the horizontal control point locations, make sure to have the 31st control point at the center of the image horizontally.