DLPU082C August 2021 – March 2024 DLPC7540
The DLPC7540 systems provide the option of an auto-initialization batch file that can be included in the flash image using the DLPDLC-GUI. The auto-initialization batch file allows the user to specify a set of commands (as described in this document) to be executed at system startup (such as booting up in Splash display mode or fixed video input for fast boot up time etc). The firmware executes the command specified in this batch-file in the specified order after it completes its own initialization procedure.
This feature provides allows the user to pre-configure the system to consistent set of powerup conditions.