DLPU112 October 2021 DLPC6540
| Issue | Probable Cause | Resolution |
|---|---|---|
| Unable to open the EVM GUI | Corrupted settings file | Find and delete the EVM's settings XML file (example DLPC2010LC.xml) which is located at user's AppData\Roaming\Texas Instruments\DLP EVM GUI folder |
| External Video does not display or does not display correctly | Unsupported video resolution |
Check the External source's resolution and make sure it is supported/with-in-range of the EVM GUI's resolution |
| GUI does not connect to the DLP471TP EVM | The EVM GUI will try to connect to the EVM automatically. However, for the DLP471TP EVM, the user has to connect to the EVM for the first time manually. | Select the communication interface and make the connection manually through the Connection page in the Debug tab. Once connected, the GUI will remember the connection settings and will auto-connect during startup. |
| Simple mode for the DLP471TP EVM does not work after opening advanced mode | Only one application can be connected to the DLP471TP EVM at a time | Go to the connection page in the advanced mode and click disconnect. After disconnecting in the advanced mode, manually connect to the EVM from the Debug > Connection page in the simple mode. |