SBAA378B November 2019 – December 2023 PCM3140-Q1 , PCM5140-Q1 , PCM6140-Q1 , TLV320ADC3140 , TLV320ADC5140 , TLV320ADC6140
A Digital Biquad Filter is a second-order IIR filter with two poles and two zeros. Biquad is an abbreviation of biquadratic. Thus, a Digital Biquad Filter is an IIR filter whose transfer function is the ratio of two quadratic functions given by Equation 2 and the corresponding direct form II block diagram shown in Figure 2-1. In this equation, the coefficients are normalized so that a0 = 1 through the division of all the coefficients by a0.

Figure 2-1 Direct Form II Biquad Filter