SBAA378B November 2019 – December 2023 PCM3140-Q1 , PCM5140-Q1 , PCM6140-Q1 , TLV320ADC3140 , TLV320ADC5140 , TLV320ADC6140
To facilitate the use of the Digital Biquad Filters, the PurePath™ Console includes a graphical filter design section that plots the magnitude, phase, and group delay versus frequency. This filter design also generates the coefficients through several different filter design techniques filters. Equation 3 shows the available filter design options with a short description of the filter type. In Table 3-1, the cutoff frequency refers to the frequency when the response changes by 3 dB from the passband.
| FILTER TYPE | DESCRIPTION |
|---|---|
| Band Pass | Band-Pass filter at the specified center frequency and passband width (filter bandwidth) |
| Bass Shelf | Specified gain applied at the low frequency up to the specified cutoff frequency |
| Equalizer (Bandwidth) | Band-pass filters at the specified center frequency and passband width, with the specified gain |
| Equalizer (Q Factor) | Band-pass filter at the specified center frequency and quality factor, with the specified gain. The quality factor is the center frequency divided by the passband width. |
| Gain | All pass filter at the specified gain |
| High-Pass Butterworth 1 | First-order high-pass filter with specified gain, specified cutoff frequency, maximally flat passband and stopband response. Stopband frequency response has a –10 dB / decade slope. |
| High-Pass Butterworth 2 | Second-order high-pass filter with specified gain, specified cutoff frequency, maximally flat passband and stopband response. Stopband frequency response has a –20 dB / decade. |
| High-Pass Bessel 2 | Second-order high-pass filter with specified gain, specified cutoff frequency, maximally flat phase and constant group delay across passband. |
| High-Pass Linkwitz Riley 2 | Second-order high-pass filter composed of a Butterworth filter with –3 dB at the cutoff frequency. When cascading a low-pass and high-pass Linkwitz Riley filters, the overall gain at the crossover frequency is 0 dB. |
| High-Pass Variable Q 2 | Second-order high-pass filter at the specified center frequency, gain, and quality factor. The quality factor is the center frequency divided by the passband width. |
| High-Pass Chebyshev | High-pass filter with equiripple in the passband with maximally flat response in stopband |
| Low-Pass Butterworth 1 | First-order low-pass filter with specified gain, specified cutoff frequency, maximally flat passband and stopband response. Stopband frequency response has a –10 dB / decade slope. |
| Low-Pass Butterworth 2 | Second-order low-pass filter with specified gain, specified cutoff frequency, maximally flat passband and stopband response. Stopband frequency response has a –20 dB / decade. |
| Low-Pass Bessel 2 | Second-order low-pass filter with specified gain, specified cutoff frequency, maximally flat group delay across passband |
| Low-Pass Linkwitz Riley 2 | Second-order low-pass filter composed of a Butterworth filter with –3 dB at the cutoff frequency. When cascading a low-pass and high-pass Linkwitz Riley filters, the overall gain at the crossover frequency is 0 dB. |
| Low-Pass Variable Q 2 | Second-order low-pass filter at the specified center frequency, gain and quality factor. The quality factor is the center frequency divided by the passband width. |
| Low-Pass Chebyshev | Low-pass filter with equiripple in the passband with maximally flat response in stopband |
| Notch | Band stop filter at the specified center frequency and stopband width (filter bandwidth) |
| Phase Shift | All pass filter with 180 degree phase shift at the specified center frequency through the width given by the bandwidth |
| Treble Shelf | Specified gain applied at the high frequencies past the specified cutoff frequency |