SBAA729 August 2025 AFE7900 , AFE7901 , AFE7903 , AFE7906 , AFE7950 , AFE7951 , AFE7953 , AFE7954 , AFE7955 , AFE7958
Device bringup of AFE79xx device is generally done using micro controller through SPI. In some of the applications, micro-controller can not be allowed in the system. For such applications, HDL based device bringup is needed to configure the AFE. Texas Instruments BRINGUP_AFE HDL module integrated into the FPGA along with a memory (to store the bringup instructions) can be used to configure AFE79xx devices.