SBAU232A October   2020  – November 2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Device Information
  8. 2Hardware
    1. 2.1 Required Hardware
    2. 2.2 Hardware Setup
  9. 3Software
    1. 3.1 Required Software
    2. 3.2 Software Setup
  10. 4Setup Procedure
    1. 4.1 Setting up the ADC3660EVM
    2. 4.2 Setting up the ADC3644EVM
    3. 4.3 Setting up the ADC3643EVM
  11. 5Hardware Design Files
  12. 6Additional Information
    1. 6.1 Trademarks
  13. 7References
  14. 8Revision History

Setting up the ADC3643EVM

  1. Verify that the software is set up according to the Software Setup section.
  2. Verify that the hardware is set up according to the Hardware Setup section
  3. To provide the CLK signal:
    1. Using an SMA cable and an inline 65MHz band pass filter, connect the signal generator to the CLKp SMA connector (J5) on the ADC3643EVM.
    2. Set the output signal frequency of the signal generator to 65MHz and the signal amplitude to +10dBm.
  4. By default, the EVM is configured to take a single ended input, so analog inputs must be applied to connectors CHAp (J7) for Channel A or CHBp (J9) for Channel B. To provide an analog input:
    1. Using an SMA cable and an inline 5MHz band pass filter, connect the signal generator to analog input channel A.
    2. Set the output signal frequency of the signal generator to 5.135MHz (prime number) and 0dBm.
  5. To provide a DCLK signal:
    1. Using an SMA cable, connect the signal generator to the DCLKIN SMA connector (J6).
    2. Set the output frequency of the signal generator to 227.5MHz (14-bit, 2-wire, DDC bypass) and the signal amplitude to +2dBm.
  6. Verify that all signal generators for clock, analog input and DCLK are referenced locked using the 10MHz REF on the back of the signal generators. For an example of this, please see figure below.
    ADC3660EVM, ADC3644EVM, ADC3643EVM Basic Test Measurement SetupFigure 4-17 Basic Test Measurement Setup
  7. Your setup now looks like the following:
    ADC3660EVM, ADC3644EVM, ADC3643EVM ADC3643EVM Hardware Setup Figure 4-18 ADC3643EVM Hardware Setup
  8. Open HSDC Pro. Always verify that HSDC Pro is open before opening the ADC36xxEVM GUI.
  9. Select on cancel when prompted to connect to a board. The GUI handles all of the other HSDC Pro capture and configuration related operations.
    ADC3660EVM, ADC3644EVM, ADC3643EVM HSDC ProFigure 4-19 HSDC Pro
  10. Open the ADC36xxEVM GUI. Allow a few seconds for the GUI to connect to the TSWDC155EVM FPGA Capture board. The TSWDC155EVM powers on, and several LEDs become illuminated, as shown below.
    ADC3660EVM, ADC3644EVM, ADC3643EVM TSWDC155EVM Powered On Figure 4-20 TSWDC155EVM Powered On
  11. Once the GUI is opened, verify that the correct ADC mode parameters are selected, then click on the “Calculate” button to calculate the necessary DCLK. For this mode, the DCLK must be 227.5MHz. Verify that this signal is provided to the DCLK input on the hardware setup.
    ADC3660EVM, ADC3644EVM, ADC3643EVM Calculating DCLK Frequency for
            ADC3643 Figure 4-21 Calculating DCLK Frequency for ADC3643
  12. Select the “Program” button. Allow a few seconds to program the ADC, program the FPGA, and configure the FPGA firmware.
    ADC3660EVM, ADC3644EVM, ADC3643EVM Programming the ADC3643EVMFigure 4-22 Programming the ADC3643EVM
  13. Once programming is complete, select the "Capture" button to take an FFT data capture.
    ADC3660EVM, ADC3644EVM, ADC3643EVM Capturing the FFTFigure 4-23 Capturing the FFT
  14. After a few seconds, the captured data appears in the HSDC Pro window, where you can view the performance of the device. For more functions and features of HSDC Pro, see the HSDC Pro User Guide.
    ADC3660EVM, ADC3644EVM, ADC3643EVM ADC3643EVM FFT Data Capture in HSDC
            Pro Figure 4-24 ADC3643EVM FFT Data Capture in HSDC Pro
  15. If an error occurs when running the capture function, restart the GUI and follow steps 5-8 again.