SBAU394A April   2022  – September 2022

 

  1.   ADS1285 Evaluation Module
  2.   Trademarks
  3. EVM Overview
    1. 1.1 ADS1285EVM-PDK Kit
  4. ADS1285EVM-PDK Quick-Start Guide
  5. EVM Analog Interface
    1. 3.1 ADC Analog Input Signal Path
    2. 3.2 ADC Input Clock (CLK) Options
  6. Digital Interface
    1. 4.1 Connection to the PHI
    2. 4.2 Digital Header
  7. Power Supplies
  8. Digital-to-Analog Converter
  9. ADS1285EVM-PDK Initial Setup
    1. 7.1 Default Jumper Settings
    2. 7.2 EVM Graphical User Interface (GUI) Software Installation
  10. ADS1285EVM-PDK Software Reference
    1. 8.1 EVM GUI Global Settings for ADC Control
    2. 8.2 Register Map Configuration Tool
    3. 8.3 Time Domain Display Tool
    4. 8.4 Spectral Analysis Tool
    5. 8.5 Histogram Tool
    6. 8.6 DAC Configuration Tool
  11. ADS1285EVM-PDK Bill of Materials, PCB Layout, and Schematics
    1. 9.1 Bill of Materials
    2. 9.2 PCB Layout
    3. 9.3 Schematics
  12. 10References
  13. 11Revision History

ADC Input Clock (CLK) Options

Using the onboard oscillator, clock dividers, and external connectors, the ADS1285EVM-PDK has device configuration flexibility. The ADC operates from CLK, which generates the modulator clock (fMOD), provided in one of two ways:

  • A crystal oscillator and the accompanying clock dividers can provide a selectable frequency for the entire range of the ADC.
    • The onboard crystal oscillator (Y1) provides the nominal 8.192-MHz clock frequency (default)
    • The dividers (U6) step down the frequency to 4.096 MHz
    • J8 allows the user to select between these frequencies and connect them directly to CLK by using a shunt
  • An external main clock can be provided to a subminiature version A (SMA) connector (J5) or to pins 4 or 2 of J7 when a shunt does not select the frequency from the crystal oscillator.
    • In this case, a shunt must not cover J7 so that CLK is connected to any of the crystal oscillator signals
    • Be sure to review the valid CLKIN input frequency in the data sheet
Note: All clock sources are sourced back to the PHI connector (J6) so that the GUI SCLK communication is synchronous with CLK.

Figure 3-2 shows a schematic for the clock source.

GUID-20220830-SS0I-XV5K-ZGND-0TRFZJCCL5V0-low.gif Figure 3-2 CLK Source (Schematic)