SBAU431A July 2024 – October 2026
The time domain display tool allows visualization of the ADC response to a given input signal. Use this tool to study the behavior and debug any gross problems with the ADC or drive circuits. Access this page by selecting Time Domain Display under Pages on the left side of the GUI.
Trigger a capture of the data of the selected number of samples from the ADS1282 EVM, as per the current interface mode settings indicated in Figure 4-7 by using the Capture button. The sample indices on the x-axis and the y-axis show the corresponding equivalent analog codes or voltages based on the specified reference voltage. Switching pages to any of the analysis tools described in the subsequent sections causes calculations to be performed on the same set of data.