SBAU431A July 2024 – October 2026
The histogram analysis tool, shown in Figure 4-9, calculates the maximum, minimum, peak-to-peak, mean and sigma (standard deviation) on a DC input data set. Access this page by selecting the Histogram Analysis under Pages on the left side of the GUI.
Noise degrades ADC resolution and the histogram tool can be used to estimate effective resolution. The cumulative effect of noise coupled to the ADC output comes from sources such as the input drive circuit, reference drive circuit, ADC power supply and the ADC. Cumulative noise is reflected in the standard deviation of the ADC output code histogram obtained by performing multiple conversions of a DC input applied to a given channel. Figure 4-9 shows the histogram corresponding to a DC input displayed by clicking the Capture button.