SBAU436B January 2024 – February 2025
Figure 2-6 shows the buffer circuit for the ADC VCOM signal. The output of the VCOM buffer connects to the VOCM signal of the input driver amplifiers. The J1 VCOM header pins (depopulated by default) can also be used to provide an alternate source for VCOM by depopulating resistor R5. Jumper J1 can also be used to connect the VCOM signal to an external piece of test equipment to set the common-mode voltage. A common use case is to connect this signal to the Audio Precision SYS-2722 to set the signal generator's common-mode output.