The ADS1278EVM-PDK includes the
following components, as shown in Figure 1-1.
- The PHI controller board.
- The ADS1278 EVM board which
includes the ADS1278 and peripheral circuitry required for device operation and
communication with the PHI board.
- An A-to-Micro-B USB cable for
communication between the PHI board and the EVM GUI.
- The EVM GUI, which can be found
online in the EVM tool folder.