To set up the GUI the first time, follow
these steps:
- Make sure that the previously-mentioned
driver is installed successfully to verify everything works properly.
- Plug the connected EVM and SCB unit to the
PC and go to the GUI link provided earlier.
- Select the GUI Composer application window
shown in Figure 3-4 to launch the GUI from
the web browser.
- For first-time GUI Composer setup,
follow the prompts to download the TI Cloud Agent and browser extension shown
in Figure 3-5. These prompts
appear after you close the README.md dialog.
- Select the
icon in the GUI Composer window shown in Figure 3-4 to download the GUI
offline (optional).