2.3.1.4 Test Case 4: Connect Signal Generator
Output Port to RX of the AFE7769DEVM (at output power, -23dBm)
Once the steps in "Initial
bringup for all test cases" section are complete, navigate to the
Channel-Controls tab in Latte and under the “Channel TDD” box, click the buttons
for RX to turn them green and “Set Tdd”, as shown in Figure 2-10.
Connect any of the RX ports (RX1
= J1, RX2 = J2, RX3 = J3, TX4 = J4) from the AFE7769DEVM to the RF output of the
signal generator.
Ensure the signal generator is
set to a frequency and output power of 1805.025 MHz and -23dBm, respectively.
Figure 2-16 Signal Generator
Settings, Test Case 4
In File Explorer, navigate to the
“test1122_txz_rxz.stp” file, and double-click to open it in Signal Tap.
Ensure “rx_datalink” is the
selected tab and row; click the boxed icon as shown in Figure 2-15 to begin running data acquisition.
Once acquisition is clear, pause
the simulation with the same icon, this time a red square.
Right-click on the
“uu00|jesd204_rx_link_data” section of the middle pane, choose “Create Signal
Tap List File”, and save as a .txt file.
Decipher the data using the
provided MATLAB script titled “rx_data_test.m”, and replace the sample .txt file
name with the newly-created .txt file from the previous step.
After running the code, a figure
with four graphs will appear.