2.3.1.1 Test Case 1: Generate Sinusoidal tx_data
From NCO @ 5MHz
Once the steps in "Initial
bringup for all test cases" section are complete, navigate to the
Channel-Controls tab in Latte and in the first section of this window, click the
buttons under TX TDD to turn them green and click “Set Tdd”.
Figure 2-10 Enable TX TDD
Monitor the power supply
connected to the AFE. The current should increase from approximately 1.2A
post-Device Bring up to 2A when TDD is enabled.
Connect any of the TX ports (TX1
= J7, TX2 = J8, TX3 = J9, TX4 = J10) from the AFE7769DEVM to the spectrum
analyzer.
Figure 2-11 represents the expected result for this test case.