This section discusses the initial
setup of the test environment, as well as the necessary power connections.
- Mount the FMC+ connector of the
AFE7769DEVM to the receiving part on the Arria 10 FPGA (labeled J19), as shown
in Figure 2-1.
- Ensure the following connections
are made to the necessary power supplies/ports, and that the Arria 10 is
switched on, as shown above. The switch can be found in the bottom-right corner
of the above figure.
- USB-C cable: connected to
PC used to launch Latte GUI.
- AFE7769DEVM Power cable:
connected to a power supply @ 5.5V
- Ethernet cable: connected
to Ethernet port
- USB Blaster cable:
connected to PC used to launch Quartus Programmer and SignalTap
- Arria 10 Power cable:
connected to safe power outlet
For all other hardware integrations
for the Arria 10, see the Intel® Arria® 10 SX SoC Development Kit.